- Stratix device properties
Clear a fault on a ring
If a rapid fault or restore cycle fault occurs on the ring supervisor, select
Clear faults
in the Ring X
view to clear the fault.
TIP:
Clear faults
is only available when the switch is a ring supervisor.To clear the fault on a ring
- On the tab for the device, expandDevice Level Ring, and then expand the appropriateRing.
- In theRing Xview, selectClear faults.
Provide Feedback