Configure ports for changes at controller

Configure ports for changes at controller

Use the
Fault/Program Action
view to configure ports for these changes at the controller:
  • The controller transitions to Program mode
  • Communication is disrupted between the controller and the switch
    TIP:
    The switch can be online or offline.
To configure ports for changes at the controller
  1. On the tab for the device, select
    Fault/Program Action
    .
  2. In the
    Fault/Program Action
    view, configure the parameters for each port as needed.
  3. Select
    OK
    to finalize the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.