- Stratix device properties
Create a new DHCP pool
Create a new DHCP address pool once the DHCP is enabled.
Prerequisites
- The device is online.
To create a DHCP pool
- On the tab for the device, selectDHCP Pools.
- In theDHCP Poolsview, select these check boxes:
- Enable Dynamic Host Configuration Protocol (DHCP)
- Enable DHCP Snooping
- Select
.
- InAdd/Edit DHCP Pool, configure the DHCP address pool properties as needed.
- SelectSetto send the changes to the switch.TIP:You may need to enter a password in theEnter Passworddialog box.
Provide Feedback