- Stratix device properties
Delete a DHCP pool
Use the
DHCP Pools
view to delete an existing DHCP pool.Prerequisites
- The device is online.
- The DHCP is enabled.
To delete an existing DHCP pool
- On the tab for the device, selectDHCP Pools.
- In theDHCP Poolsview, select the checkbox of the pool or pools that you want to delete, and then select
.
- In the confirmation dialog box, selectDelete.All persistent addresses associated with the selected DHCP pool are also deleted.
Provide Feedback