Edit a DHCP pool

Edit a DHCP pool

Use the
DHCP Pools
view to edit the properties of an existing DHCP pool.
Prerequisites
  • The device is online.
  • The DHCP is enabled.
To edit an existing DHCP pool
  1. On the tab for the device, select
    DHCP Pools
    .
  2. In the
    DHCP Pools
    view, select the checkbox for the pool you want to edit, and then select edit .
  3. In
    Add/Edit DHCP Pool
    , modify the parameters as needed.
  4. Select
    Set
    to send the changes to the switch.
    TIP:
    You may need to enter a password in the
    Enter Password
    dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.