- Stratix device properties
Export the switch configuration
Once the switch configuration is uploaded from the switch to the project, the switch configuration can be exported as computer files. Depending on the model, the switch configuration may consist of a single config.text file or config.text and vlan.dat files. Use the
Save/Restore
view to export the switch configuration.Export
is not available if there is no switch configuration to export.Prerequisites
- The device is online.
To export the switch configuration to files
- On the tab for the device, selectSave/Restore.
- In theSave/Restoreview, selectExport.
- For Logix Designer inExport, browse to the folder where you want to store the configuration, enter a File name for the ZIP file containing the configuration, and then selectSave.For FactoryTalk Design Studio inExport Device Configuration, selectExportand thenNextfor each file to be exported. Select For FactoryTalk Design Studio in Export Device Configuration, selectExportand thenNextfor each file to be exported. SelectClosewhen finished.
TIP:
The file is saved to your browser's
Downloads
folder.Provide Feedback