- Stratix device properties
Import a switch configuration
Restore a switch configuration by importing the switch configuration from files stored on the computer. The switch configuration includes the config.text file and the vlan.dat file.
To import the switch configuration files
- On the tab for the device, selectSave/Restore.
- In theSave/Restoreview, selectImport.
- For Logix Designer in the selection dialog box, select the one or more configuration files as listed in the dialogue box's title, and then selectOpen.For FactoryTalk Design Studio in the Import dialogue box, selectBrowse, select the configuration file, selectOpen,and then selectNextfor every configuration file. After the last configuration file is selected, clickImport.TIP: To download the imported configuration to the switch, selectDownload.
Provide Feedback