Reset the port diagnostic counters

Reset the port diagnostic counters

Use the
Port Diagnostics
dialog box to reset the interface and media counters to zero to assist in troubleshooting issues.
Prerequisites
  • The device is online.
  1. On the tab for the device, select
    Port Status
    .
  2. In the
    Port Status
    view, in the
    Port Diagnostics
    column for the port, select FTDStudioPortDiag.
  3. In
    Port Diagnostics
    , select
    Reset counters
    .
    The interface and media counter values on the device reset to zero and the values displayed in the dialog box update with the current counter values.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.