- Stratix device properties
Reset the ring fault counter
Reset the switch's ring fault count to zero to assist in troubleshooting issues.
Prerequisites
- The switch is online and is a ring supervisor.
To reset the ring fault counters
- On the tab for the device, expandDevice Level Ring, and then expandRing X.
- SelectReset counters.Ring faults detectedresets to zero, and the value displayed in the view updates with the current counter value.
Provide Feedback