- Stratix device properties
Sort ring members
Sort the members of the ring by IP address or MAC address. These columns are marked with the arrow icon (
or
).


To sort ring members in ascending and descending order
- On the tab for the device, expandDevice Level Ring, and then expandRing X.
- SelectMembers.
- In theMembersview, select the arrow of theIP AddressorMAC Addresscolumn header to alternate between ascending and descending order.
Provide Feedback