Verify the last fault location on a port

Verify the last fault location on a port

When there is a fault on a ring, you can see the last node the active ring supervisor can communicate with on a DLR port. This information displays in
Last Active Node
in the
Ring X
view.
TIP:
Last Active Node
shows information from the last fault until you verify the fault location.
To verify the last fault location on a port
  1. On the tab for the device, expand
    Device Level Ring
    , and then expand
    Ring X
    .
  2. In the
    Ring
    view, select
    Verify fault location
    .
    The switch updates the IP address or MAC ID in
    Last active node on Port 1
    and
    Last active node on Port 2
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.