Ring X view

Ring X view

Use the
Ring X
view to enable the switch as a ring supervisor, and view information about the network and ring.
Use the
Ring X
view to:
  • Enable supervisor mode on the ring.
  • View whether the switch is operating in a DLR or linear network.
  • View the status of the network.
  • View the address and the precedence of the active ring supervisor.
  • View the current status of the supervisor.
  • View the number of ring faults, the status of the ring fault, and clear the rapid fault or restore cycle fault.
  • Reset the ring fault count to zero.
  • View the address of the last active node on the ports when there is a fault.
Data displays and the parameters are available only when the device is online and there are no communication errors.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.