Configure the DLR network

Configure the DLR network

Use the
Device Level Ring
view to configure the DLR network. DLR is available on select switch models and ports.
Prerequisites
  • The switch is online and communicating.
  • The switch is operating on a ring network.
To configure the DLR network
  1. On the tab for the device, select
    Device Level Ring
    .
  2. In the
    Device Level Ring
    view, in the
    Enable
    column for the Ring, select the checkbox to enable DLR on the switch ports.
  3. Select the ring ports for
    Port 1
    and
    Port 2
    .
    TIP:
    Port 1
    and
    Port 2
    cannot be set to the same port. Once a port is selected, that port is not available to the other port.
  4. Select
    Set
    to send the settings to the switch.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.