- Stratix device properties
Assign a precedence value to the ring supervisor
Use the
Advanced Network Configuration
dialog box to assign a precedence value to the ring supervisor.To assign a precedence value to the ring supervisor
- On the tab for the device, expandDevice Level Ring, and then selectRing X.
- In theRing Xview, selectEnable Supervisor Mode.TIP:The configuration takes effect immediately.
- SelectAdvanced.
- InAdvanced Network Configuration, in theSupervisor precedencefield, enter a precedence value between 0 and 255.TIP:
- Configure the desired active ring supervisor with a numerically higher precedence value as compared to the back-up supervisors.
- The precedence is transmitted in beacon frames.
- (optional) Enter values for these two parameters:
- Beacon interval
- Beacon timeout
- SelectSet.
Provide Feedback