EtherChannels view
Use the
EtherChannels
view to view information about EtherChannels. An EtherChannel, or port group, is a group of two or more Fast Ethernet or Gigabit Ethernet switch ports that are bundled into a logical link. The group creates a higher bandwidth link between two switches. For example, four 10/100 switch ports can be assigned to an EtherChannel to provide full-duplex bandwidth of up to 800 Mb/s. If one of the ports in the EtherChannel becomes unavailable, traffic is carried over the remaining ports within the EtherChannel.Use the
EtherChannels
view to:- View the EtherChannel groups.
- View the mode.
- View the port members assigned to each EtherChannel.
- View the status of the port members.
Provide Feedback