- Stratix device properties
Fault/Program Action view
Use the
Fault/Program Action
view to configure each port on the switch for changes at the controller. Use this view to:- Determine the behavior at each port when the controller transitions to Program mode.
- Determine the behavior at each port when the connection from the controller to the switch is disrupted.
Provide Feedback