NAT view
Use the
NAT
view to create and modify Network Address Translation (NAT) instances. A NAT instance contains entries that define each address translation, as well as other configuration parameters.In the
NAT
view, you can:- Delete a NAT instance.
- Create a NAT instance.
- Edit an existing NAT instance.
- View diagnostics information about a NAT instance.
- View diagnostics data for all NAT instances.
TIP:
The parameters in this view are available while online.
Provide Feedback