- Stratix device properties
New Entry dialog box parameters
The
New Entry
dialog box includes these parameters:Parameter | Description |
---|---|
Number of Entries Available | Displays the number of translation entries available on the switch. The switch supports a maximum of 128 translation entries. |
Type of Entry | Defines the type of entry to add to the translation table.
|
Starting Public IP Address | Specifies the public address or the starting address for the device(s). The Public IP address needs to be unique. There can be duplicates in different NAT instances, but not in the same instance. The same Public IP address can appear in both the Private to Public NAT Table and Public to Private NAT Table of the same instance. An invalid Starting Private IP Address results in Effective Private Addresses field to be blank.If the Type of Entry is Subnet , Starting Public IP Address must correspond to the size of the subnet mask. See more details in Starting Public IP Address. |
Starting Private IP Address | Specifies the existing address or the starting address for the device(s) on the private subnet. The Private IP address needs to be unique. There can be duplicates in different NAT instances, but not in the same instance. The same Private IP address can appear in both the Private to Public NAT Table and Public to Private NAT Table of the same instance. An invalid Starting Private IP Address results in Effective Private Addresses field to be blank.If the Type of Entry is Subnet , Starting Private IP Address must correspond to the size of the subnet mask. See more details in Starting Private IP Address. |
Range | Specifies the number of addresses to include in the range. Valid values are 1..128. The default value is 1. Tip : Each address in the range counts as one translation entry. The switch supports a maximum of 128 translation entries. |
Subnet Mask | Specifies a list of valid subnet masks for the addresses to translate. Valid values:
|
Effective Public Addresses | Displays the unique public address or range of unique public addresses to represent the devices. |
Effective Private Addresses | Displays the existing address or range of existing addresses for devices on the private subnet that are configured for translation. |
Provide Feedback