- Stratix device properties
Add NTP Server dialog box
Use the
Add NTP Server
dialog box to add an NTP server address to the NTP Servers
table. When the NTP server address is added, the server provides the time source to the NTP client.Provide Feedback