Add an NTP server address

Add an NTP server address

Use the
Add NTP Server
dialog box to add an NTP server address to the
NTP Servers
table.
Prerequisites
  • The device is online.
  • NTP is enabled on the device.
To add an NTP server address
  1. On the tab for the device, select
    NTP Client
    .
  2. In the
    NTP Client
    view, select add.
  3. In
    Add NTP Server
    , enter the server address, and then select
    OK
    .
  4. Select
    Set
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.