- Stratix device properties
Delete an NTP server address
Use the
NTP Client
view to delete an NTP server address from the NTP Servers
table.
IMPORTANT:
Deleting all NTP server addresses disables the NTP client functionality and makes the switch no longer have an external NTP time source.
Prerequisites
- The device is online.
- NTP is enabled on the device.
To delete an NTP server address
- On the tab for the device, selectNTP Client.
- In theNTP Serverstable, select the checkbox for the NTP server address you want to delete, and then select
.
- In the confirmation dialog box, selectDelete.
Provide Feedback