Configure the NTP client

Configure the NTP client

Use the
NTP client
view to configure the switch as an NTP client to one or more servers.
Prerequisites
  • The device is online.
  • NTP is enabled on the device.
To configure the NTP client
  1. On the tab for the device, select
    NTP Client
    .
  2. In the
    NTP Client
    view, add NTP servers as needed.
  3. Select
    OK
    to finalize the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.