Port Thresholds view
Use the
Port Thresholds
view to set the Incoming and Outgoing threshold limits for broadcast, unicast, and multicast traffic for each active port. These limits help determine acceptable levels of performance.If an undesirable network event occurs and the threshold value is exceeded, a yes value displays in two places:
- the appropriate column in thePort Statusview
- theTraffic Exceeded on Any Portparameter in theSwitch StatusviewTIP:Configure the port threshold settings while online. Most data is only displayed when the device is online.
Provide Feedback