Switch Status view

Switch Status view

Use the
Switch Status
view to monitor the switch and port conditions to quickly see if a fault or error condition exists. This view also shows the overall health of the switch (temperature and power).
TIP:
The parameters in this view are available while online.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.