- Stratix device properties
Time Sync Configuration view
Use the
Time Sync Configuration
view to synchronize the ports through Time Sync Configuration. Time Synchronization synchronizes with nanosecond accuracy the real-time clocks of the devices in a network. Using the best master clock selection, the switch identifies the switch port that is connected to a device with the best clock source. The switch then synchronizes its internal clock with the best clock source and the switch port is set to master state. The most precise clock source in the network is referred to as the grandmaster clock.The data is only displayed when the device is online. To configure time synchronization, the device must be online and the
Time Sync Enable
check box is selected.Provide Feedback