Diagnose a problem with a device
Use
Device Diagnostics
to diagnose a problem. Diagnostics is disabled when:- You are operating offline.
- An Identity mismatch exists.
To diagnose a problem with a device
- On the tab for the device, selectDevice Information.
- In theDevice Informationview, selectDiagnostics.
- InDevice Diagnostics, view the diagnostics for the device.
Provide Feedback