Device Diagnostics parameters

Device Diagnostics parameters

Device Diagnostics
is used for multiple device types so the parameters displayed can vary. Settings that do not apply to a device type do not appear.
TIP:
When the connection is lost to the device, a timeout error occurs. On dismissal of the error message, the parameters are blank.
Select
Retry communication
to update the data in the dialog box.
Device Diagnostics
includes these parameters:
Parameter
Description
Value
Run mode
Shows the operating state for the device. Run Mode is blank when the device is offline, or when the connection is not established to the device.
Output devices follow the Run Mode for the owning connection.
Input-only devices are always in Run Mode.
0 = Idle
1= Run
Diagnostics threshold exceeded
Shows whether any diagnostics are active or a threshold has been reached when the event occurred.
0 = No diagnostics active
1= One or more diagnostic thresholds reached
Diagnostics sequence count
Shows the count for each time a distinct diagnostic condition was detected, and also each time a distinct diagnostic condition transitioned from detected to not detected.
-128...127
The value of 0 is skipped except during device power-up.
Self test
Shows whether the product initialization code detected an error.
0 = Passed
1 = Failed
CPU utilization
Shows the usage of the compute engine.
0% to 100%
Connections
Shows the number of CIP connections currently open to and through the adapter.
0 to 32767
Packets lost
Shows the running sum of the number of Sequenced Address Item Sequence Numbers that are skipped in Class 0 and Class 1 connections consumed by the adapter and its children.
0 to 2147483647
Timeout
Shows the running count of the number of connections that time out, both originated and targeted, to and through the adapter.
0 to 2147483647
Time synchronization - Status
Shows whether the device is currently synchronized with a 1588 master.
0 = Not synchronized with a 1588 master
1 = Synchronized with a 1588 master
Grand master clock identity
Shows the identity of the Grand Master clock to which the device is synced.
8-byte hex number
Local clock offset to system time
Shows the offset, in nanoseconds, from the local clock to the system time.
Use this value to detect steps in time. This value updates when a Precision Time Protocol (PTP) update message is received.
-9223372036854775808 to 9223372036854775807
Local clock offset timestamp
Shows the timestamp of the local clock offset in YYYY-MM-DD-HH:mm:SS.mmm format.
  • YYYY = year
  • MM = month
  • DD = day
  • HH = hour (24 hour)
  • mm = minutes
  • SS = seconds
  • mmm = milliseconds
A valid time or blank if no event time has been recorded.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal