Modifying the Hierarchy

Modifying the Hierarchy

It helps the user to modify the hierarchy structure by moving the hierarchy node.
NOTE: When a new node is added in Active status at Asset Setup, a message is displayed to inform users to set it as zero for the newly created active node. The user can click
Define Weightage
to navigate and realign the weightage. If a node is created in a non-active state, only a node is created and no need to define weightage for the non-active state node.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.