Import Hierarchy

Import Hierarchy

This functionality applies from Enterprise to Asset levels but not for the Component level. Perform the following steps to Import Hierarchy:
  1. On the left navigation menu, drop-down the
    Configuration
    menu and click
    Asset Setup
    .
  2. Click the required node from the Hierarchy list.
  3. Click the [] icon and select
    Import Hierarchy
    .
    Select Import Hierarchy
  4. In the
    Import Hierarchy
    window, click
    Browse
    .
  5. In the pop-up window, select the required file and click
    Open
    .
  6. The
    Hierarchy Preview
    is available on the right side of the window and click
    Import
    .
    Import Hierarchy Window
    The "
    Hierarchy.xml imported successfully
    " message is displayed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.