Change the default CodeMeter configuration

Change the default CodeMeter configuration

By default CodeMeter dongles attempt to connect to the CodeMeter time server over the Internet to verify the certified time that is included in their license files. In an environment where computers are not connected to the internet this behavior can cause slower performance. Therefore, if a computer will not be connected to the Internet and is using a CodeMeter dongle to store activations, we recommend changing the default CodeMeter configuration to improve performance. 
To change the default CodeMeter configuration
  1. Click
    Advanced > Configure CodeMeter
    .
  2. Click
    WebAdmin
    to open the
    CodeMeter WebAdmin
    console.
  3. Click
    Configuration > Advanced
    to open the
    Time Server
    page (http://localhost:22352/configuration/certified_time.html)
  4. By default four URLs are listed in the
    Time Server
    list.
    CodeMeter Time Server list
  5. Click
    Remove
    CodeMeter Remove Icon next to the URL and remove all but one of the time servers.
  6. Click in the
    Time Out
    box and change the value to 1 second. This action decreases the time spent by the software attempting to connect to the time servers from 80 seconds (4 x 20 seconds) down to 1 second.
    If the computer networking is changed to be connected to the Internet, press the
    Restore Defaults
    button to return the time servers to the default configuration.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal