Advanced FactoryTalk Activation server settings

Advanced FactoryTalk Activation server settings

How do I open the Advanced page?
From
FactoryTalk Activation Manager
, click the
Advanced
tab.
Use the
Advanced
page to:
  • Refresh activation servers running on the computer
  • Configure CodeMeter settings on this computer
  • Configure Websocket Server settings
  • Configure Automatic Renewal settings
  • Access the Activation Folder
  • Open the Diagnostics Viewer
  • Edit the Options file
  • Show bindings available for this computer
  • Borrow and return activations using a data file
If you are not using CodeMeter dongles for activation, you can also:
  • Create activations manually
  • Rehost activations manually
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal