File access settings

File access settings

How do I open the File Access page?
Click
Advanced > File Access
.
Use the
File Access
page to:
  • Browse to the Activation folder.
    Click
    Browse Activation Folder
    to open Windows Explorer scoped to the activation folder. This folder contains the Options file, activation files, and the
    Logs
    folder where server log files are stored.
  • View
    FactoryTalk
    Diagnostics.
    Click
    View Diagnostics
    to open the
    FactoryTalk
    Diagnostics Viewer. This viewer displays the event messages from all of the
    FactoryTalk
    system components. Click a message to view details. The log file is cleared when the server is refreshed or restarted.
  • Edit the Options file.
    Click
    Edit Options File
    to open the options file (flexsvr.opt) in Notepad for editing. The options file is used to configure special circumstances for activation clients. By default, the options file is blank.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.