Data available in an activation-related message
The Diagnostic Viewer displays the following information. Some types of data are available only for specific types of transactions. The example information in the following table is for a
borrow return
transaction type.Data | Description | Borrow return example |
Transaction | Type of action requested by FactoryTalk Activation Manager . | borrow return |
Server | The computer that requested the transaction. | LocComp2 |
Feature | The activation feature/file name that is being used. | RSVSESRV.250 |
Version | Product version number. | 3.00 |
Serial number | Serial number of the product. | 2322888888 |
Other | ||
Severity | Severity of the message such as Information, Audit, Error, Warning. | Information |
Audience | Type of user and security. | Operator & Secured |
Time | Date and time the diagnostic information was logged. | 7/2/2015 3:14:56 PM |
Location | Name of computer where the diagnostic message was generated. | RemComp1 |
Provider | Service that provided the data to be logged. | FactoryTalk Activation Server |
User | User domain and login name, or domain and computer name, or SYSTEM depending on the transaction type. | SYSTEM |
Full Name | Full name of the logged in user, or blank. | blank |
Provide Feedback