View messages in FactoryTalk Diagnostics Viewer

When an activation is borrowed or returned,
FactoryTalk Activation Manager
sends a message to the
FactoryTalk Diagnostics
log identifying the user who borrowed or returned the activation.
Activation-related messages are logged to
FactoryTalk Diagnostics
Viewer only on the local computer by default.
To view messages in
FactoryTalk Diagnostics
Viewer:
  1. Click
    Advanced
    >
    File Access
    .
  2. Click
    View Diagnostics
    to open the
    FactoryTalk Diagnostics
    Viewer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal