Create or edit the Options file

The
Options
file is a text file that defines the options for managing concurrent activations.
To create or edit the Options file:
  1. Click the
    Advanced
    tab, and click
    File Access
    .
  2. Click
    Edit Options File
    to open the file in a text editor.
  3. Type the lines into the options file as needed to control the activation servers response to an activation request.
  4. Save the file with the name
    flexsvr.opt
    in the default activation folder.
  5. Restart the activation service to implement the new options.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.