Check activation server status
Use
Activation Server Status
to:- Verify the status of activation servers.
- Determine if an activation server is unresponsive, needs software updates, or needs activations renewed.
To check the status of activation servers:
- At the right of the taskbar at the bottom of the screen, click the up arrow to show hidden icons.
- Click theRockwell Activationicon
.
- ClickCheck Servers Now. TheActivation Server Statusbox lists the name of the activation servers and the status of each server. A server can be in the following states:
- Unresponsive. Indicates that the computer is not communicating with the activation server due to a problem with the server or the connection to the server.
- Needs update. Indicates that the server is not running the latest version ofFactoryTalk Activation. Contact your system administrator to install the current version ofFactoryTalk Activation.
- ClickClose.
Provide Feedback