Configure the FactoryTalk Activation server

Configure the FactoryTalk Activation server

The
FactoryTalk Activation
server manages and shares activations with other configured computers on the network. Multiple activation servers can exist on a network, and client computers can retrieve activations from more than one activation server. A remote computer can also be set as an activation server.
The
FactoryTalk Activation
server does not require a server operating system, and can be any computer that hosts activations for distribution to clients. However, a server operating system will administer the licenses more effectively. Download times will be shorter and the system administrator can use a single, central computer to host activations.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.