View the server log file

View the server log file

The server log file is generated each time an activation server is started or refreshed.
To view the server log file:
  1. Start the activation server if it is not already running.
  2. Navigate to the server log directory. The default directory is
    C:\Users\Public\Documents\
    Rockwell Automation
    \Activations\Logs\
    .
  3. Open the server log file
    RSsvr.log
    in a text editor.
    Tip:
    When viewing the log file, ignore references to RSI.MASTER.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.