Restart the activation services

Restart the activation services

Restart the
FactoryTalk Activation
services if you cannot refresh the server using the
Refresh
button, or if activations do not appear after adding an activation server.
To restart the activation services:
  1. Open the
    Windows
    Control Panel
    , then click
    Administrative Tools > Services
    .
  2. Right-click
    FactoryTalk Activation
    Helper
    , and click
    Restart
    .
  3. Right-click
    FactoryTalk Activation
    Service
    , and click
    Restart
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal