Create or update a data file
A data file contains the binding information of a computer.
To create or update a data file:
- At the computer without Internet access, attach a removable storage device, openFactoryTalk Activation Manager, and clickManage Activations.
- ClickGet New Activations.
- ClickI need to start the activation process by creating a data file.
- ClickSpecify Data File.
- The default location forFactoryTalk Activation Managerdata files is listed inFile Locationand the default data file name is listed inFile name. ClickBrowse
to navigate to a different storage location. If the data file exists, click the file to choose it.
- ClickGet Bindings.
- To select a binding for the computer, do one of the following:
- Accept the default binding.
- Select a different binding. To view a list of bindings currently in the data file, clickShow Collected Bindings.
- (optional) Enter a name for a binding, by clicking inNameand entering the name.
- ClickCreate Data File.FactoryTalk Activation Managercreates or updates the XML data file at the specified location.
Provide Feedback