Download an activation to a removable storage device
To get an activation for a computer that doesn't have Internet access, take the disconnected computers data file to a computer with Internet access and then use that computer to download an activation to a removable storage device.
Before you begin:
A removable storage device with a copy of the disconnected computer's data file is required.
For each product being activated, have the following:
- Product serial number
- Product key
- The earliest version of the product to activate (when multiple versions of a software product are being installed).
To download an activation to a removable storage device:
- At a computer with Internet access, attach the removable storage device.
- Open theFactoryTalk Activation ManagerHomepage, clickGet New Activations.
- Enter the serial number and product key for the software being activated and clickValidate Activationto open theValidate Activationtable.
- (optional) For each product in theValidate Activationtable, theProduct Versioncolumn displays the earliest version of the product available. Use this default value or select a different version.
- To download more than one copy of the activation, edit the value in the# to Downloadcell. After the earliest version selections have been validated, theBindingcells become active and display the default binding.
- Select the binding that includes the disconnected computer's data file:
- Click in theBindingcell.
- ClickBrowse
to open the
Binding Selectionwindow. - In theBinding Selectionwindow, clickImport Additional Bindingand then choose XML data file you created.
- ClickSelectto accept the binding and close theBinding Selectionwindow.
- ClickDownload Activation.
- After the activations have downloaded, clickPrintto save a copy of the activation information for your records.
Provide Feedback