Move an activation to a computer without Internet access
After downloading activations to a removable storage device, move the activations to the computer that is not connected to the Internet.
Before you begin:
- Download activations from an Internet-connected computer to a removable storage device.
To move an activation to a computer without Internet access:
- Attach the removable storage device that includes the downloaded activations to the target computer.
- On theFactoryTalk Activation Managerhome page, click theManage Activationstab.
- ClickGet New Activations.
- ClickI have downloaded activation files and need to move them to this computer.
- ClickSpecify File Location. TheFile locationbox displays the location of the file on the removable storage device. Click theBrowsebutton to select a different location.
- ClickMove Filesto import the files and activate the licenses.
Provide Feedback