Rehost an activation from a computer with Internet access

Rehosting an activation removes the activation from either the current host computer or dongle and returns it to the pool of activations on the activation server.
For concurrent activations with a quantity greater than 1, there is the option to select a quantity less than the total activations. This leaves a quantity of the activations on the local computer while allowing the rest of the activations to become available for download to other computers. By default, all activations are removed from the local computer.
Before you begin:
  • If rehosting a dongle-based activation, insert the dongle into the USB port of the Internet connected computer.
To rehost an activation from a computer with Internet access:
  1. Click
    Manage Activations
    >
    Rehost Activations
    .
  2. Select the checkbox next to the activation to rehost.
  3. If more than one activation is available, in
    # to Rehost
    , enter the number of activations to rehost. By default, all activations are rehosted.
  4. Click
    Continue Rehosting
    . The
    Confirm Activation Removal
    dialog box opens.
  5. Click
    Continue
    to complete the rehosting or click
    Cancel
    to return to
    Select Activations
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.