Rehost Activations page

Rehost Activations page

How do I open Rehost Activations?
Click
Manage Activations > Rehost Activations
.
Rehost activations for unexpected or infrequent events, such as a computer upgrade, system failure, or changes to the system.
Use the
Rehost Activations
page to remove an activation from its current host computer to move it to a different computer. Rehosting is not intended for moving activations frequently.
TIP:
Rehost activations to remove expired activations from the host computer.
For concurrent activations with a quantity greater than 1, there is the option to select a quantity less than the total activations. This leaves a quantity of the activations on the local computer while allowing the rest of the activations to become available for download to other computers. By default, all activations are removed from the local computer.
If moving the activation between computers that have an internet connection
, use
FactoryTalk Activation Manager
to rehost an activation automatically. The rehost code is automatically created and sent to the
Rockwell Automation
Licensing website.
If moving the activation from a computer that is not connected to the internet
, to complete the process, use another Internet-connected computer to connect to the
Rockwell Automation
Licensing website.
If rehosting with no computers connected to the internet
, contact
Rockwell Automation
Technical Support to perform the rehosting process.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.