Rehost an activation from a computer without an Internet connection
Rehosting an activation removes the activation from the current host device and returns it to the pool of activations on the activation server. If the computer using the activation does not have an Internet connection, transfer the activation data file to a removable storage device and take it to a computer with Internet access to perform the rehosting process.
On a computer without an Internet connection, you cannot select a quantity of activations less than the total number of activations. All activations are removed from the local computer.
TIP:
Both the computer connected to the Internet and the computer disconnected from the Internet must run the same version of
FactoryTalk Activation Manager
.To rehost an activation from a computer without an Internet connection
- On the computer without an Internet connection, attach the storage device and startFactoryTalk Activation Manager. Select the activations to rehost using the following steps:
- ClickManage Activations>Rehost Activations.
- On theChoose Phasepage, selectI need to select the activations I want to bind to a different computer or dongleand clickSelect Data File.
- On theSelect Data Filepage, create the data file to use for rehosting. Use the default file name (FTAManagerData.xml) and location. Or, specify a different file name and location in theFile locationbox by clickingBrowse
to navigate to and select the file. Or, type the name and path of the file directly in the space provided.
- ClickSelect Activations. In the activations table, select theProductcheckbox for each activation to rehost.
- ClickNext Steps. A confirmation window lists the selected activations. ClickContinueto proceed, or clickCancelto end the procedure without removing the activations.
- On theNext Stepspage, clickGo to Data File Locationto open the file folder in Windows Explorer. Copy the data file to a removable storage device.
- Go to a computer with an Internet connection. Transfer the activations to the pool of activations using the following steps:
- ClickManage Activations>Rehost Activations.
- ClickImport From Data File. By default the data file copied to the removable storage device is selected. ClickOpen. Select the checkbox next to the activations to rehost.
- ClickContinue Rehosting. TheConfirm Activation Removaldialog box opens. ClickContinueor clickCancelto return to theSelect Activationspage. TheContacting Rockwell Automation Activation Serviceprogress bar appears while the activations are being processed. The data file is updated to indicate that the activations have been rehosted.
- Return to the computer without an Internet connection, attach the removable storage device, startFactoryTalk Activation Managerand perform the following steps to finish the rehosting process:
- ClickManage Activations>Rehost Activations.
- On theChoose Phasepage, selectI need to remove rehosted activations from this machineand clickSelect Data File.
- Select the name and location of the data file on the removable storage device and then clickNext Steps. The confirmation dialog opens. ClickContinueto complete the removal of the activation.
- Go to a computer with an Internet connection. Transfer the activations to the pool of activations using the following steps:
- ClickManage Activations>Rehost Activations.
- ClickImport From Data File. The removable storage device is selected. ClickOpen. Select the checkbox next to the activations to rehost.
- ClickContinue Rehosting. TheContacting Rockwell Automation Activation Serviceprogress appears during the process.
Provide Feedback