Rehost an activation when Internet access is not available
Rehosting an activation removes the activation from the current host and returns it to the pool of activations on the activation server.
On a computer without an Internet connection, you cannot select a quantity of activations less than the total number of activations. All activations are removed from the local computer.
If Internet access is not available, call
Rockwell Automation
Technical Support to rehost the activation file.
IMPORTANT:
CodeMeter
-based activations cannot be rehosted manually.To rehost an activation when Internet access is not available:
- ClickAdvanced>Rehost Activation Manually.
- Select the checkboxes next to the activations to rehost.
- ClickComplete Rehosting. A confirmation dialog box opens.
- ClickContinueto remove the activation files from this computer, or clickCancelto end the process without removing the activations.
- ClickPrintto print the information forRockwell AutomationTechnical Support.
- CallRockwell AutomationTechnical Support at the number listed on theComplete Rehostingpage for a guide through the steps to rehost activation files.To return to theSelect Activationspage, clickRehost Activation Manually.
Provide Feedback