Run the FactoryTalk Activation Command-line Utility
Use the
FactoryTalk Activation
Command-line Utility to script operations such as getting and rehosting activations or configuring the activation search path.To run the
FactoryTalk Activation
Command-line Utility- Run a command prompt as an administrator.
- Set the command prompt path to theToolsdirectory in the install location. For example:C:\Program Files (x86)\Rockwell Software\FactoryTalk Activation\Tools.
- EnterFTACmdUtility.exe.TIP:To see more information about a command, enterFTACmdUtility.exe <command> -h.
Provide Feedback