Command-line utility return values

Command-line utility return values

A list of all the possible return values from the FTACmdUtility tool.
Return values
Return value
Description
0
Command completed successfully.
1
Required FTACore.dll was not found or failed to load.
2
FTAScript interface is not supported in the loaded FTACore.dll.
3
ReflectionTypeLoadException thrown attempting to obtain FTAScript interface.
4
General Exception thrown when attempting to obtain FTAScript interface.
5
Unexpected error occurred determining whether standard user is allowed to execute command.
6
Dispose of the FTAScript interface unexpectedly failed.
7
Get of the activation search path unexpectedly failed.
8
Add of an activation search path unexpectedly failed.
9
Remove of an activation search path unexpectedly failed.
10
Get all local bindings failed.
11
Get activations failed.
12
Get rehost data failed.
13
Rehost failed.
14
Renew failed.
15
Manual rehost failed.
16
Writing binding information to the transport file failed.
17
Invalid contents of transport file when writing binding information.
18
Import of activation files failed.
19
Write of rehost data to the transport file failed.
20
Write of renew update data to the transport file failed.
21
Write of rehost update or renew data to the transport file failed.
22
Import of the rehost or renew data failed during disconnected rehost/renew.
23
Confirmation of the disconnected rehost failed.
24
Borrow of an activation failed.
25
Return of an activation failed.
26
MissingMethodException thrown when calling FTAScript interface method.
27
General Exception thrown when calling FTAScript interface method.
28
A disconnected borrow is not implemented.
29
Validation of borrow activation data failed.
30
Current user not allowed to run command.
31
Configure Clear Always Fail command failed.
32
Configure Clear Feature Group command failed.
33
Configure Show Always Fail command failed.
34
Configure Show Feature Group command failed.
35
Configure Feature Group command failed.
36
Configure Always Fail command failed.
37
Connection to RADAR web-service failed. Command requires connection.
38
Confirmation of the connected rehost failed.
39
Get command failed.
40
Import of the connected rehost failed.
41
Import of the connected renew failed.
42
List Available Activations failed.
43
Creation of FTAScript interface failed.
44
Parsing of command line parameters threw exception.
45
General exception thrown during command processing.
46
General exception thrown during FTAScript method execution.
47
Connected rehost failed unexpectedly.
48
Disconnected rehost failed unexpectedly.
49
Manual rehost failed unexpectedly.
50
Disconnected return of an activation failed.
51
Validation of return of an activation failed.
52
Write to transport data file of rehost or renew update data failed.
53
Get FTA versions failed.
54
General parsing failure.
55
selectBorrowDestination command failure.
56
selectBorrowSource command failure.
57
importBorrow command failure.
58
confirmBorrow command failure.
59
selectReturnSource command failure.
60
writeReturnUpdate command failure.
61
importReturn command failure.
62
confirmReturn command failure.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal