Configuration

Configuration

Perform the following steps to configure the FTA Activation Service:
  1. Go to
    FTActivationWebSocket
    folder:
    C:\Program Files (x86)\Rockwell Automation\FactoryTalk Activation Websocket Service
  2. Open the
    WebsocketService.dll.config
    file and add the following information:
    IMPORTANT:
    Ensure that proper permissions are provided to access certificates folder.
    • Certification.file:
      Provide the <FQDN-hostname>.p12 file directory path.
      NOTE:
      Refer to the “Generate Certificate” chapter to generate certificate.
    • Certification.password:
      Provide the keystore password.
    • Certification.passwordEncryption
      : The default value is false. Upon stop and start of the service, the private key will be encrypted.
    • Port:
      Port number where Websocket Service is running.
      Config file
  3. Save and close the
    WebsocketService.dll.config
    file.
  4. Stop and start the FT Activation WebSocket Service.
    Restart FT Activation WebSocket Service
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal