Generate Certificates in Windows
In Distributed mode, the DataView, FTASecurity, and FTA Activation Service can be installed on different machines. To establish a connection between DataView server, FTASecurity server, and FTA Activation Service, use the following scenarios to generate certificates as applicable.
- FTASecurity and FTA Activation Service installed on same machine.
- FTASecurity and FTA Activation Service installed on different machines.
Provide Feedback